6/21/2021 8:12 PM | |
Joined: 6/6/2021 Last visit: 8/26/2024 Posts: 9 Rating: (0) |
Hi all I have DMG DMC 63V MACHINE WITH siemens 810d controller and getting a problem with spindle motor over temperature error but the temperature will be only 52 degree Celsius we even checked the sensor and even replaced it with new one but too the problem is same fan is also working fine am not getting exactly what problem it has sensor and wires are all fine error code 511104 spindle motor over temperature at only 52 degrees ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/22/2021 08:51:33New subject after splitting |
|
6/22/2021 6:50 AM | |
Joined: 6/6/2021 Last visit: 8/26/2024 Posts: 9 Rating: (0) |
KTY 84 SENSOR SPINDLE MOTOR 1PH7107 |
6/22/2021 7:47 AM | |
Joined: 6/6/2021 Last visit: 8/26/2024 Posts: 9 Rating: (0) |
Resistance is .59 to .6 ohms and ill attach the drive image |
Last edited by: Angad Jayant Walvekar at: 06/22/2021 07:49:38 |
|
Follow us on