6/23/2021 9:09 PM | |
Posts: 1 Rating: (0) |
Hello, I am working on a DMG ecoMill 1035V. Currenly, I'm struggling with a piece in the 4th axis. On Fusion 360 it's working perfectly, but when I open it in the machine the program doesn't look so good. The first part is ok, after turning 180 degrees it is milling elsewhere. I only have some basic knowledge about G-code, not enough to identify the problem. Hope I can find help here! Attachmentezyzip (2).zip (89 Downloads) |
Last edited by: Livia0408 at: 06/29/2021 08:58:44 |
|
6/27/2021 5:20 AM | |
Joined: 9/6/2014 Last visit: 7/22/2024 Posts: 209 Rating: (6) |
. |
Follow us on