10/16/2021 12:56 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello dao hieu, Please check below points. 1. Please check & note the LED status on RMI-Q interface & compare it with healthy & erretic operation. This LED status will help you to dianosis the issue. 2. Check probe connection with 840D SL NCU. How much is the cable length? Is shileded cable used & shielding connection is correct? Is any joint provided? Is this interface cable laid nearby power cable? 3. Check if there are heavy vibrations during tool change operation, e.g. when probe is carried away. Heavy viabrations may cause loose connection in probe batteries. 4. Are you well familiar with STYLUS center & triger force adjustment? If yes, check those, if not get help from expert.
Yes, if you restore or reload NC data, (please note before you reload/restore NC or PLC data, you need to clear NC/PLC data first), you need to redefine axes reference/home zero positions. Hope this helps. |
Follow us on