10/19/2021 7:16 PM | |
Joined: 3/6/2019 Last visit: 4/18/2022 Posts: 44 Rating: (6) |
Hey guys! Due to customer requirements, I have some P&ID's in which pipelines must be colored according to service. Also in order to fulfill client's specifications, pipe flags must be present but always in black color. Unfortunately, my pipe flags seem to inherit the pipe object's color (figure 1). the pipe flag symbol I'm using is the one in figure 2. How can I make the flag's color independent from the pipe's color? I've tried explicit adding "Header.Color = RGB(0,0,0)" to the flag's symbol script, but it doesn't affect the color inheritance. Thanks! Attachmentfigures.zip (207 Downloads) |
10/20/2021 5:31 PM | |
Joined: 3/6/2019 Last visit: 4/18/2022 Posts: 44 Rating: (6) |
It works! Cheers! |
Follow us on