10/21/2021 11:06 AM | |
Joined: 12/22/2015 Last visit: 4/13/2023 Posts: 2 Rating: (0) |
Hello, My first time creating a new topic. I always find a solution to my problems here but not this time. :( We have a KTP700 Basic PN ( this one ), firmware 13.0.1.0. Program with TIA Portal V14 SP1. I would like to export the .csv file of the recipe to an USB stick. I made a button with the system function "Export Data Records" and the path is "\USB_X60.1\Recette.csv". I tried other path name I usually use on other panels but TIA goes red and only accept "USB_X60.1" (which is the path given by the help assistant). Problem is when I press the button, there are system error messages telling the path cannot be find. USB stick is FAT32 16Go. No matter if I connect the USB stick when the panel is on or off. It should be really easy, I'm not trying to do a complexe thing. Just want to export a .csv file to an USB drive as I did on other panels... But this one giving me hard time and I don't understand why. My last idea was to convert everything to TIA V17 and update the firmware to a 17 version but the machine will not be available long enough to do it before some time... and I'm not even sure it will solve the issue. Best regards, bflorian. |
Follow us on