10/20/2021 7:15 PM | |
Joined: 9/19/2017 Last visit: 11/19/2022 Posts: 3 Rating: (0) |
HI Guys. Good afternoon. I'm young here. It's my first participation in the forum. I'm having a problem to load the nc and plc.arc in 840D PowerLine. When I create the backup file, all is good but, when I need load the backup files to NCU(first the NC.ARC), the PLC.ARC is loaded but, the CPU stay in stop mode. In CPU diagnose, I can see the problem is the PLC doesn't load DB' 38, 39 and 40(Axis that I don't have in the machine). Can anyone help me about that? Best Regards Ricardo Rugeri ------------------------------------------------------------------------------------------ |
Last edited by: Ricardo Rugeri at: 10/20/2021 19:15:46Last edited by: The Helping Hand at: 10/21/2021 06:56:52New subject after splitting |
|
10/21/2021 3:15 PM | |
Joined: 9/19/2017 Last visit: 11/19/2022 Posts: 3 Rating: (0) |
Hi Raman. I saw the MD 20070 and my machine have 7 axis. The MD20070 is with 7 axis too |
10/21/2021 8:39 PM | |
Joined: 10/17/2007 Last visit: 9/17/2024 Posts: 4031 Rating: (353)
|
let me know the real reason you doing back up and reloading . just for practice ? or machine lost parameters normally if back up when machine in good working condition --you will not have trouble to reload nc/plc arc back to system. This way is tested more hundred time in my services cases for 840D PL you have idea--1st Ax using DB31 and so on. if machine has no 8th to 10th AX it will not need DB38.39 40 let me know what happen? Another tip: I think you have SIMATIC Manager --S7 programming sw. you can make DB38,DB39, DB40 (can copy paste from exiting DB31 or ..) load them into PLC to see what happen
|
Last edited by: nulizhang at: 10/21/2021 20:51:21Last edited by: nulizhang at: 10/21/2021 21:25:22Last edited by: nulizhang at: 10/30/2021 23:41:53If you like my comments please |
|
Follow us on