11/13/2021 3:02 PM | |
Joined: 1/4/2019 Last visit: 6/1/2024 Posts: 60 Rating: (0) |
dear the attached file is hardware configuration |
11/14/2021 10:46 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello engineer; Congratulations on making this network function once more. If ever you have trouble with a repeater on a futurer project, make sure how the termination resistprs on the repeater are setup, they can throw you for a loop quite easily (catch you off guard). Look at the different configurations you can create with a repeater in the manual link below, the most likey (based on your description) would be shown in the screenshot below: https://support.industry.siemens.com/cs/ww/en/view/48598071/26165387019 The basic principle is that all segments of the Profibus network need t be adequately terminated, or the Profibus signal will not travel from the first segment to the second one. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/15/2021 12:01:03 |
|
This contribution was helpful to1 thankful Users |
Follow us on