11/18/2021 12:49 PM | |
Posts: 1 Rating: (0) |
Dear all, i want to commission 2 dc Simoreg drive without encoder and i want to send setpoint via its analog input. so i have to know: 1- how can i ass https://omegle.onl/ ign on of Analog input of CUD as a main setpoint 2 - how can i define max speed of the m vshare otor without encoder 3- how can assign some of DI as start command please determine for me the major parameter that i have to change them or a procedure to commission the drive in this way. |
Last edited by: AdamZampa at: 11/23/2021 16:33:00 |
|
11/18/2021 12:59 PM | |
Joined: 8/25/2006 Last visit: 4/24/2024 Posts: 2203 Rating: (277)
|
What is the drive? 6RAxx? |
Follow us on