11/22/2021 6:02 PM | |
Joined: 10/29/2021 Last visit: 3/4/2022 Posts: 5 Rating: (0) |
I have a new challenge where I need to enable siemens S7 PLC to read data coming from a Chiller. The Chiller is using BACnet Protocol. Need a converter to convert from BACnet to a protocol that the PLC would understand. Do I need BACnet to Profinet Converter or BACnet to Modbus Converter? What is the Siemens converter part number I need to buy for this need? apparently, there are many converters in the market but I don't want to take any risk. Thanks for the answer in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/23/2021 10:58:03New subject after splitting |
|
11/22/2021 6:33 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello Hisham Halifah; You could look onto the PN/Bacnet link, 6BK1621-0AA00-0AA0. The PN/Bacnet link allows the S7 PLC to retrieve data from Bacnet devices attached to the link. The manual for the PN/Bacnet link can be downloaded here, It is the best source of information on this module (for configuration, setup, programming and troubleshooting): https://support.industry.siemens.com/cs/ww/en/view/109752591 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/23/2021 11:46:36 |
|
This contribution was helpful to1 thankful Users |
Follow us on