11/29/2021 12:34 AM | |
Posts: 4 Rating: (0) |
Dear Expert I have Siemens S7 314C-2DP CPUlast week we were running on live production when suddenly got a fault on the PLC it automatically go to stop and give SF error on cpu. I hooked up on the PLC and opened the diagnostic buffer I attached the diagnostic buffer errors, thanks and a lot and hope you guys can help me to resolve this issue AttachmentDiagnostics palletizer 4.txt (368 Downloads) |
11/30/2021 1:12 AM | |
Posts: 4 Rating: (0) |
when I checked the program there is no OB82 also compare it to the other machine Ob82 is not existed on the program |
Follow us on