12/2/2021 10:58 AM | |
Joined: 2/17/2020 Last visit: 4/19/2024 Posts: 990 Rating: (169) |
Hi xhaner, This license would be valid only to run Runtime on the PC. If you are also going to develop the project (Engineering), you will also need a Micro, Compact, Standard or Advanced WinCC Flexible license. To see the MLFBs of each one, I recommend you to check the ordering data included in the release note of the software: Delivery release: Service Pack 5 for SIMATIC WinCC flexible 2008 Note: if the engineering PC is going to be the same as the Runtime PC, perhaps the engineering license will suffice. |
A rating will be well appreciated. |
|
Follow us on