12/2/2021 7:01 AM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (139) |
Hi Phucxdtd, Microsoft Office add-in to the computer is a prerequisite for adding the reports in Microsoft Excel, and for creating and editing reports in Excel and to get the multifunction toolbar. (See the attached screenshot for your reference Excel in IS.PNG) There are two options: • You have already installed the Microsoft Office add-in when you installed the SIMATIC Information Server. • You install the add-in directly from the Web application via the "Download" app. Note the requirements for the installation Note: If there is no connection to the Information Server, check if an appropriate license is available or if there are network problems. If necessary, repeat the connection procedure. If there is no connection to the Information Server, the commands in the multifunction toolbar are not activated. Kindly go through the Section 3.8 Office add-in below manual link Information Server SIMATIC Information Server Hope it helps you! |
Last edited by: Techno_Taru at: 12/02/2021 10:34:56 |
|
This contribution was helpful to1 thankful Users |
Follow us on