12/1/2021 2:53 PM | |
Joined: 9/14/2017 Last visit: 4/5/2024 Posts: 6 Rating: (0) |
Hi, I'm trying to make a change to the Simotion Scout program version 5.3. Below are the steps I made and what happened at the end. - First thing I did was go offline and added a Global Variable B_BatchEnd (Bool) - Then performed a save project and compile changes - After saving and compiling changes there were about 6 routines that showed as mismatch with the red/green connector symbol. So I downloaded the project and all connectors went green but the program doesn't function. The tag added wasn't used just created. The HMI only shows hashtags as if the data is incorrect or not present. Attached are images of the steps taken. AttachmentScreenshots.zip (442 Downloads) |
Last edited by: Tbalt at: 12/01/2021 14:56:43Last edited by: Jen_Moderator at: 12/02/2021 08:50:08Added all files as a zip file. |
|
Follow us on