11/24/2021 2:45 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi BenjaBW, have a look into the manual CPU-CPU communication with Simatic controller All possible communication methods are described there. Consider that Profinet is a protocoll that runs on ethernet. That means when you talking about Profinet, there is already a communication running. Maybe you can be a little bit more specific. Also the term "ET200SP". Is it a IO-Device, as a decentral station(IM155-6) or an other PLC, like S7-1512SP? Also name the modules you are talking of. Which RS-485 modules do you have exactly? hope this helps, regards, |
Last edited by: mopS04 at: 11/24/2021 14:47:45FCK WAR! |
|
Follow us on