12/3/2021 6:32 AM | |
Joined: 1/17/2019 Last visit: 8/4/2022 Posts: 6 Rating: (0) |
Thanks for your comments. But Shared device is not working |
Last edited by: Abhiboss at: 12/03/2021 11:55:38 |
|
12/3/2021 11:57 AM | |
Joined: 1/17/2019 Last visit: 8/4/2022 Posts: 6 Rating: (0) |
Does it is possible to communicate two plc through PnPn coupler at X2 Side. |
12/6/2021 3:06 AM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
yes it is, see chapter 6.2.5 of the manual for all the gory details of shared device with MSI and MSO. |
Cheers |
|
12/9/2021 2:07 AM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
In that case I suggest you haven't configured the shared Device correctly (or perhaps not at all). Back to basics though, is this a V3.x or V4.x PN/PN Coupler? If so, it does support shared Device and the previously linked manual has the info in it. In addition chapter 5.3 of the PROFINET with Step 7 manual is worth studying. If still no good, you really need to provide more detail on how you configured it all. |
Cheers |
|
Follow us on