1/9/2022 4:58 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
Hallo Freek91, here the program. AttachmentLooplicht_1-4.zip (641 Downloads) |
1/9/2022 10:30 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
You also can use the program in attachment, this use another concept for the patterns. The sequence, the repeats and the patterns are all selected with pulse relays, which are cascaded to a binary counter. The first 3 pulse relays build the sequence counter (0..7), the next 2 pulse relays build the repeats (4x) and the last 2 pulse relays build the pattern selection. The patterns are stored in the parameter V1-V4 of analog multiplexers. The selection comes from the last 2 puls relays. The sequence of each pattern is selected with the 3 first pulse relays and a decoder. Q1 needs a value 1, Q2 needs a value 2, Q3 needs a value 4 and Q4 needs a value 8. To combine more then 1 output, just add the values, 5 = 1(Q1 and 4(Q3), 15 = all outputs on, 0 = all outpus off. There are used comparators to reduce the number of blocks, therefore you have to use a negative value for multiplexers connected to AY. The running lights are expandable as required, good luck. Regards, Scorp AttachmentRunning light2.zip (593 Downloads) |
1/17/2022 8:19 PM | |
Joined: 12/31/2021 Last visit: 1/30/2022 Posts: 7 Rating: (0) |
Hello ixo65, I looked at the program and changed the patterns. There are two bugs in the program: - When switching from 'Patroon 1 buiten binnen versneld' to 'Patroon 2 binnen buiten versneld' Q1 turns on for just a fraction. I want it to turn directly to Q4. - The same counts for the transition between 'Patroon 2 binnen buiten' and 'Patroon 3'. In this case Q4 turns on for a fraction before it switches to 'Patroon 3'. I tried to fix this myself, but unfortunately I don't get it. Can you've a quick look at it? Freek AttachmentLooplicht ogen.zip (610 Downloads) |
1/17/2022 8:23 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
Have you tested the programm only in simulation or in a real LOGO!? |
1/19/2022 6:58 PM | |
Joined: 12/31/2021 Last visit: 1/30/2022 Posts: 7 Rating: (0) |
Only in simulation mode in Logo!Soft |
1/19/2022 7:02 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
Then test it in a real LOGO!. Simulation is not real life ... |
Follow us on