4/22/2010 12:55 PM | |
Posts: 19 Rating: (0) |
Hi! It is possible to create two different TCP/IP connections in WinCC V7.0? Thank you |
4/22/2010 3:11 PM | |
Posts: 1 Rating: (0) |
Yes, it is possible. Just add two groups in TCP/IPchannel of SIMATIC S7 PROTOCOL SUITEand set IP addresses, Rack, Slot. |
4/22/2010 3:29 PM | |
Posts: 19 Rating: (0) |
Sorry, I expressed myself badly. I wanted to say I need two drivers TCP / IP, since one of them did not want to be updated with the cycles of PLC. Thank you |
7/23/2020 12:36 PM | |
Joined: 12/26/2016 Last visit: 9/8/2021 Posts: 2 Rating: (0) |
Hello! Try to read this topichttps://support.industry.siemens.com/tf/ww/en/posts/wincc-and-two-network-cards/151704/?page=0&pageSize=10! Solution is in the last message! I faced with the same trouble and the solutiond helped me! It is amazing, but in Set PC/PG tool both my adapters are active simultaneously. Also in WinCC in TCP/IP connection only one board can be selected. But they both are working, when runtime is launched! |
1/23/2022 3:43 PM | |
Joined: 1/23/2022 Last visit: 1/23/2022 Posts: 1 Rating: (0) |
Hello! could you send a screenshot of your pc/pg settings? I still can't do it like you |
Last edited by: MalkolmUT at: 01/23/2022 15:43:45 |
|
Follow us on