12/31/2010 10:41 AM | |
Posts: 13 Rating: (0) |
Hi, I plugged in CPU 414-2, and the INTF led on the CPU is lit up. The diganostic buffer text file and a snapshot of the diagnostic buffer is in the attached zip foler. Kindly advise on the matter. Regards,. Regards, frb AttachmentCPU414-2.zip (232 Downloads) |
1/2/2011 10:41 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Try this http://support.automation.siemens.com/WW/view/en/23579734 Best regards, Hristo Mihalev |
1/2/2011 5:44 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi, Which version do you have of STEP7? If it is some older then you might not have the CPU 414 in your catalog.... It might be possible to update your STEP7 version or you might be download the Hardware Support Packages from internet. STEP 7 Hardware Support Packages (HSPs - as at 12/2010) for installing hardware updates in the Hardware Configuration |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on