7/11/2013 12:33 PM | |
Posts: 515 Rating: (56) |
hi, find the attached architecture which might help you.
AttachmentS7 412-5H ARCHITECTURE.pdf (430 Downloads) |
7/11/2013 1:01 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, If you are willing to use S7-400 IOs, please note the following points:
Two Options are possible:
Please note that standard PS is different than PS suitable for redundant operations. Here's bellow an example:
Hope this helps. Attachmentbrochure_simatic-controller_en.pdf (275 Downloads) |
Last edited by: Ayman Elotaify at: 7/11/2013 1:02 PMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
7/11/2013 1:07 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Dear both Shazin and Ahmed, To finalize this subject.
Hope it will helps. |
Last edited by: Ayman Elotaify at: 7/11/2013 1:11 PMAyman Elotaify |
|
This contribution was helpful to2 thankful Users |
Follow us on