5/22/2014 1:11 PM | |
Posts: 4 Rating: (0) |
Please, AS 412-5H, ET200M and PC on the same Ethernet. could this configuration work? |
5/22/2014 1:42 PM | |
Joined: 7/2/2008 Last visit: 9/25/2024 Posts: 928 Rating: (308) |
Hellomiroman, The answer is YES. Look at page 33 inConfiguration Examples for S7-400H with PROFINET SIMATIC S7-400H as of V6.0. Best regards, H-H
|
This contribution was helpful to2 thankful Users |
5/23/2014 2:24 PM | |
Posts: 4 Rating: (0) |
Yes Amit_86, I meant that CP1613 is sufficient. Sorry. |
This contribution was helpful to1 thankful Users |
5/23/2014 6:33 PM | |
Joined: 7/2/2008 Last visit: 9/25/2024 Posts: 928 Rating: (308) |
Hello Everone, I just would like to clarify the important piece of info given byKhaled_Ezzatto eliminate any confusion.
It's not much related to the release of SIMATIC Net V8.2 SP2 as much as it's related to the modification that Siemens madecouple of months agoto the current productSOFTNET-IE S7 REDCONNECT VM V8.2(6GK1704-0HB08-2AA0)that was released only for virtualized environments.
Best regards, H-H
|
This contribution was helpful to2 thankful Users |
5/31/2014 8:43 PM |
|
Joined: 6/8/2013 Last visit: 7/18/2024 Posts: 158 Rating: (9) |
Yes it is possible |
Follow us on