4/19/2016 11:57 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please refer attached cycle83. Also attaching drill tool parameter data. I think drill which is called in your program is something special tool, c edge - might be cutting edge. AttachmentDrill tool .zip (200 Downloads) |
4/19/2016 10:22 PM | |
Joined: 10/17/2007 Last visit: 4/22/2024 Posts: 3972 Rating: (340) |
I think you have more knowledge about "Cutting technology" than I . My advantage is electrical and electronics, of cause Siemens CNC/PLC/Drives as well. this time you have couple of doubts, I just answer some as I know. --Link is download "manual Cycles" you can read how to set up Cycle83--I suggest you try Cycle 81 1st, then cycle83, make sure you have all Siemens cycles loaded into CNC memory --check program-cycle--to see all cycles have check mark after loaded[x] https://support.industry.siemens.com/cs/attachments/109439500/PGZ_0400_en.pdf --"Base" data in Tool offset--just left it empty, it is just give user some options and flexibilities. --you can think it is tool adaptor . --And as I know if you input a tool as drill , normally will only think about ONE length compensation , not like mill tool thinking radius as well. if you find and download the 840D programming I post in last week, you will find description for tool offset. For G83 I will check and answer you in next post PS:if you download the whole book "Cycles" there is example for cycle 83--see my attached pic
|
Last edited by: nulizhang at: 4/19/2016 10:35:49 PMadd example cycle83 Last edited by: Min_Moderator at: 4/20/2016 10:40:07 AMEdit link to permanent one If you like my comments please |
|
4/20/2016 11:32 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please refer the attached sheet which may help you. I guess, this is the manual you are looking for. SINUMERIK 840D/840Di/810D ShopMillAttachmentSlot milling .pdf (189 Downloads) |
Last edited by: PISCEAN 2010 at: 4/20/2016 11:39:23 AM |
|
Follow us on