2/10/2017 4:16 PM | |
Posts: 88 Rating: (4) |
Help me to configure DI,DO of sinamics g120 . |
2/11/2017 5:06 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
It depends upon type of CU used. Please refer attached sheets, in this case CU is 250S-2. HTH. AttachmentSinamics G120 LV inverter chasis device with CU250S-2 control unit.pdf (91 Downloads) |
2/12/2017 3:44 PM | |
Posts: 88 Rating: (4) |
how to configure Digital output of cu 240 E |
2/14/2017 10:13 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please download & study below appliccation example. SINAMICS G120 Control Units CU240E |
2/16/2017 1:49 PM | |
Posts: 1 Rating: (0) |
hello Help me to configure DI,DO of sinamics G120 6SL3224-0BE34-5AA0 I can't found the parameter P700 |
Last edited by: touaitiwalid at: 2/16/2017 1:50:04 PM |
|
2/17/2017 7:30 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Which is CU? |
2/17/2017 11:21 AM | |
Joined: 3/31/2015 Last visit: 1/26/2024 Posts: 175 Rating: (16) |
Because there is no p700 in G120. Just use starter and save some time. There is a nice GUI to configure the I/Os |
2/20/2017 10:59 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by idop is split to a separate thread with the subject G120, can't change control. Best regards |
Follow us on