2/17/2017 10:48 AM | |
Posts: 9 Rating: (0) |
AttachmentFOUTENLIJST.pdf (182 Downloads) |
2/17/2017 11:32 AM | |
Posts: 9 Rating: (0) |
|
2/17/2017 4:15 PM | |
Joined: 2/22/2008 Last visit: 3/28/2023 Posts: 57 Rating: (6) |
Dear qsdf789, Related to ASM command, see below the answer (copied from Convert from S5 to S7-300 using IP240) "ASM is not a command but a notification that the block is protected. Siemens has written these blocks and the code are hidden. These blocks are mostly system dependent. It is therefore not necessary to convert these blocks." That instruction calls the FB which is in the EPROM of the CPU. The FB is placed in the system memory of the CPU and is in assembly. Therefore I suggest you to rewrite this function (you should know what it stands for) or use another one. |
Last edited by: Ronaldo Junior at: 2/17/2017 4:20:23 PMBest Regards |
|
This contribution was helpful to2 thankful Users |
Follow us on