11/24/2008 8:23 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hi Remove FB250 and you can use fc105 ( scale function ) for analog signals. Fb40 (PID controller). But FB40 has difference between the PID parameters in the different controller packages in STEP5 and STEP7. Just change and check parameters. Or maybe is better to use FB41. Errors in OB - see from which OB number. It's possible to receive from OB20, 21, 22, 250 or 251. OB20 Manual complete (cold) restart; OB21 Manual (warm) restart; OB22 Automatic (warm) restart; Just check what has incide and decide - delete or use in STEP7 format. This manual STEP 7 - From S5 to S7 is helpfull. regards |
6/12/2014 9:51 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, Here is the rightlink. Read it and try to solve your problem. If still problems please return with some details. Regards, Marcjan
|
Problem solved? |
|
This contribution was helpful to1 thankful Users |
3/23/2017 3:24 AM | |
Posts: 8 Rating: (0) |
Hello Marcjan, May i ask you to update the link again? Because i think that link is already broken again. Thanks. Regards, Calvin D. S. |
Follow us on