1/31/2017 12:40 PM | |
Joined: 11/29/2011 Last visit: 5/3/2024 Posts: 1357 Rating: (229) |
As nobody responded yet... It sounds like a firmware issue. Maybe try to contact Siemens Support and confirm it with them. Firmware version of the hardware can be modified, see the Operating System Update for S7-400 Standard CPUs (FW V5.1.1) article for further info. |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |
2/2/2017 11:12 AM | |
Joined: 11/29/2011 Last visit: 5/3/2024 Posts: 1357 Rating: (229) |
Hi, Just a small information you may find usefull: You do not need flash card to update firmware. See SIMATIC Configuring Hardware and Communication Connections STEP 7 V5.5 under chapter "13.1.5 Updating Firmware in Modules and Submodules Online" I hope I could help! |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |
2/3/2017 10:49 PM | |
Posts: 9 Rating: (0) |
Hi, Unfortunately I can't do this because my CPU doesn´t support the "Update firmware" function. I already asked SIEMENS about it and they told me that I realy need the memory card. Thanks for your information Romero Spinasse
|
5/23/2017 11:49 AM | |
Joined: 7/14/2016 Last visit: 9/12/2023 Posts: 387 Rating: (27) |
Hello, Is this memory reset happening in both the CPUs or only one? I had the similar problem. Turns out that problem with the sync module can erase your CPU. Please refer to my post. In your case also may be some of the faulty component is causing this memory reset? hope this helps. Kbv. |
Don't just think in terms of solutions... |
|
Follow us on