3/23/2017 11:03 AM | |
Posts: 11 Rating: (1) |
Hello, I am using Simatic .NET V14 on an IPC427E running under Windows 7 Ultimate SP1. When I load de configuration file .xdb both OPC_Server and IE_General are with a green mark a few seconds and then the IE_general moves to Stop. The diagnostic buffer shows this error:
We've tried: - Updating S.O (installing all available updates). - Updating BIOS. - Uninstalling Simatic .NET v14 and installing it again. - Uninstalling Simatic .NET v14 and installing Simatic .NET v13 - Reinstalling drivers of the network cards - Different configurations on the TIA portal project : PC Station, using the GSD for the IPC427E, using the three different network cards in the configuration - ... We've been installing Simatic .NET in docens of devices in the last years, this is the first time we face this error. Any suggestion? Thanks in advance, Kind Regards AttachmentTIA.zip (89 Downloads) |
3/23/2017 11:08 AM | |
Posts: 531 Rating: (34) |
Maybe an irq sharing issue. The CP seems to be removed, added and then reconfigurated. |
This contribution was helpful to1 thankful Users |
Follow us on