4/23/2017 11:25 AM | |
Posts: 16 Rating: (0) |
Dear all, I am using SFC in PCS7 V8.2 and apply function calculate some thing. But it is not working. see the attachment Please give a help to solve Thank |
4/24/2017 3:07 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
When this kinds of errors happen, first thing i will do is to check the version of the softwares.. Im using V8.2 too, Is it almost similar with yours? (for those that you think it is not related, just ignore it) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/24/2017 6:51 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Siemens will update their software via some updates to solve some of the bugs. If you installed from CD , that means, all the software version you having are the original one. Your case seem like a bugs. I would suggest you to contact siemens technical support https://support.industry.siemens.com/cs/ww/en/sc/2100 ( please check the installed software version that you are having too. ) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
6/21/2017 10:26 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi guys, An update is released for PCS7 v8.2: CFC update 4 which fixes an issue with sfc calculations. Maybe the problem is solved when installing the update... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on