5/16/2017 8:33 PM | |
Joined: 1/1/2017 Last visit: 4/22/2024 Posts: 329 Rating: (11) |
Dear All, I've provided the addressing as per standard only but still the CPU integrated Inputs are not responding! Can anybody suggest what may be the probable reason for this issue! I'm forcing the values in VAT table, the changes are responding in logic, but when physically I'm providing external 24VDC to the channels they are not responding in the logic! Please help me. Regards Omkris ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/17/2017 12:11:33 PMNew subject after splitting |
|
6/1/2017 11:51 AM | |
Joined: 2/11/2015 Last visit: 4/25/2024 Posts: 437 Rating: (33) |
try to not wire the outputs and force agains the output, the LED is lighting?¿ |
Follow us on