4/19/2017 7:45 AM | |
Joined: 1/2/2017 Last visit: 7/29/2024 Posts: 209 Rating: (117) |
Is query column connected to attribute? In this case list is created automatically. |
4/19/2017 8:28 AM | |
Joined: 1/2/2017 Last visit: 7/29/2024 Posts: 209 Rating: (117) |
Open attribute display. There is frame Edit field type. Is option Combobox selected?
|
4/19/2017 9:05 AM | |
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating: (42) |
Hi Jiri, Find enclosed file, for more details about issue. In attribute, list is working. But in query, use of dynamic attribute to show the list is not working. Both edit field & combobox script is defined are same. -- Regards Dinesh K AttachmentList in query - issue.pdf (479 Downloads) |
5/24/2017 10:33 AM | |
Joined: 4/28/2015 Last visit: 3/31/2023 Posts: 18 Rating: (13) |
hi, which COMOS version you used. it maybe a bug. |
Follow us on