6/24/2017 5:38 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi GUWS, Confirm whether the said block is processed by CPU [ with the help of Call structure or status display at the bottom line(Flashing green)]. This can be also due to multiple monitoring running simultaneously. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
6/29/2017 12:01 PM | |
Joined: 4/18/2014 Last visit: 3/25/2024 Posts: 253 Rating: (5) |
Dear Sir, i am monitoring in OB1 not in FB. And the plc is in RUN mode only. |
Follow us on