7/27/2017 12:08 PM | |
Joined: 6/4/2012 Last visit: 9/2/2024 Posts: 6 Rating: (0) |
Hi I have problem with fault on my CPU 315-2 DP. BF Led is on but on diagnosis buffer is no error. When I plug Profibus plug error is disappearing (wen I pushing Profibus sometimes is on sometime is off) but still no logs in buffer. PLC working normally. Only One PLC have this issue The rest PLC'S are OK. Should I replace connector? I use Profibus to connect 10pcs PLC and one "data logger" (ACCON Net Link Pro) to be able, to connect to PLC via WIFI. In Diagnosis buffer is one event about Profibus but it does not tell my nothing. any body have some ideas? AttachmentDiagnose L03A.txt (74 Downloads) |
Follow us on