9/27/2013 10:22 AM | |
Posts: 391 Rating: (50)
|
Dear chandhaa, it depends on the software version of the 840D sl. If you have software version 2.x you can still use HMI-Advanced as operator interface and your applications will still work. Maybe with minor adaptions. If you have software version 4.x then you need Sinumerik Operate as operator interface. In this case your applications will not work anymore. You need to rewrite them with the new programming package Create MyHMI/3GL , either in .NET or in C++ and Qt. Also the HMI OA option that you have to activate on the control is different. The order code is 6FC5861-1YC41-1YA0 for the latest version available 4.5 SP1 http://support.automation.siemens.com/WW/view/en/66489105 . The supported programming environment for this version is Visual Studio 2008. If you want to program with C++ and Qt you also need to buy a Qt license from www.digia.com. You will find more information on this when you buy the Create MyHMI/3GL package. |
This contribution was helpful to1 thankful Users |
9/27/2013 11:22 AM | |
Joined: 3/28/2007 Last visit: 9/15/2024 Posts: 40 Rating: (0) |
Thanks for the information APC Tech Team Chandhaa |
3/20/2014 1:05 PM | |
Posts: 340 Rating: (6) |
new question is splittet to Why have I to use so old software I mean Visual Studio 2008 ? SINUMERIK 840D sl, . |
7/30/2014 4:59 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question was split to Wincc Flexible 2008 for customised screen development in 840D SL with Sinumerik Operate. Best regards O_Moderator |
8/15/2017 10:43 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by ND120685 is split to a separate thread with the subject Software "6FC5253-7BX20-6AG0 HMI Programming Package" and "HMI Advance" - Can install in normal PC or have to install it in PCU to programming HMI?. Best regards |
Follow us on