7/27/2017 4:50 PM | |
Posts: 60 Rating: (0) |
Hello, i've made some logic that i have simocode, micromaster and starters Ds1ex to read datasets. I have ocnstant 80C3 errors, and no data. also, if i put wrong address, It gives 80A2 which may be correct and also shows that the resource is available. maybe theres someone tho give me a hand with this if you can spot if something is wrong?? Attachmentwrongaddress.txt (86 Downloads) |
Last edited by: Jen_Moderator at: 7/28/2017 2:09:00 PMPut the address in a txt file and added as an attachment. |
|
7/28/2017 8:00 PM | |
Posts: 60 Rating: (0) |
maybe some practical example? |
7/31/2017 2:04 PM | |
Posts: 60 Rating: (0) |
how is done the "DP slave diagnostics" in online hardware config - module information??? |
8/1/2017 10:00 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi martinralayer, the error-code from SFC59 80C3 means that the resources you are trying to read are currently occuppied. There is a FAQ and the description in the manual maybe helps too: System Software for S7-300/400 System and Standard Functions hope this helps, regards, |
FCK WAR! |
|
8/1/2017 7:46 PM | |
Posts: 60 Rating: (0) |
I have several SFC14 and SFC15 calls in the program, but no SFC59 calls, I don't know if these use the same resources. anyway I've changed the call in OB1 to be the first call, but again the same error 80C3... Also I've modified the code to either wait for a call with code 7000 and also tried to push execution in case 80C3 error... both ways doesn't work.... Maybe there's someone that has some sample code to use this SFC59 function working in real life... Attachmentfunction.txt (79 Downloads) |
Last edited by: Jen_Moderator at: 8/2/2017 9:10:12 AMDeleted function and added it as an attachment. |
|
Follow us on