8/16/2017 8:00 PM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello Gustavo; First point: you do not need a gsd file for an Ethernet CP. A gsd file is a configuration ocmponent por a Profibus-DP slave, so it has nothing to do with what you need. What you are looking for is a Firmware Update. Here is a link to information on the v2.7 firmware for your CP: CP 443-1 Firmware Update V2.7 and Unrestricted ... - Siemens Support You will find a link to the file download in the document above. However, I would study the following warning from the document: Please also note:If you use a current STEP 7 version (e.g. V5.4 ) you should select “FW 2.6” of the CP in the HW-Configuration of STEP 7. In this case STEP 7 will issue a warning upon loading of the configuration, relating to the difference in firmware version compared to the actually mounted hardware in the rack. This warning can be ignored with “OK“. Hope this helps, Daniel chartier |
Follow us on