10/23/2017 3:41 PM | |
Joined: 8/3/2009 Last visit: 4/23/2024 Posts: 12834 Rating: (1639) |
Hello Urantia you have to look if there is a communication driver that is suitable for this kind of PLC: https://support.industry.siemens.com/cs/de/en/pv/6AV2124-0JC01-0AX0/td -> If there is no direct communication driver you have to use a company independent communication protocol like OPC UA. So you have to use a OPC UA Server that can access the FANUC PLC and then you can use the OPC UA Client Channel of the Panel to communicate. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
Follow us on