8/4/2016 10:25 AM | |
Joined: 12/6/2007 Last visit: 3/28/2024 Posts: 12 Rating: (0) |
windows 7 ultimate sp1 64 bit step7 v5.5 sp4 |
8/4/2016 10:29 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983) |
Hi, and which WinCC? Try the following: Open Windows Device Manager
Christoph |
9/12/2017 10:13 AM | |
Joined: 3/2/2007 Last visit: 5/8/2024 Posts: 929 Rating: (5) |
" simatic filed pg m4 cp5711 " how did you solve this issue ? thank you |
... thank you ... |
|
9/12/2017 10:47 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, have you tried the suggestions from ChristophD? If no, try it? If yes, what´s the status? regards, |
FCK WAR! |
|
10/23/2017 7:55 AM | |
Joined: 3/2/2007 Last visit: 5/8/2024 Posts: 929 Rating: (5) |
yes, i tried. it is solved. the cp5711 was not appearing in the set pg/pc interface. in the device manager, it was with a yellow mark, and a message of uninstalled driver. then i installed the driver by selecting browse for it in the c harddisk . thank you for your help. |
... thank you ... |
|
10/23/2017 1:37 PM | |
Joined: 8/3/2009 Last visit: 5/8/2024 Posts: 12886 Rating: (1645) |
Hello Ziemens do you need still any help or does the CP5711 work now at your computer? It was not able to read out this information out of your last post without a doupt. Bye Murof |
If this Information really helps, you could use the Rate function |
|
10/24/2017 7:23 AM | |
Joined: 3/2/2007 Last visit: 5/8/2024 Posts: 929 Rating: (5) |
yes, it is working fine. thank you |
... thank you ... |
|
This contribution was helpful to1 thankful Users |
Follow us on