11/20/2017 3:07 PM | |
Posts: 3 Rating: (0) |
Dear All I am having a problem with IbaPDA_V.6.35.3 and PCS 7 V9.0. I managed to connect to PLC via iba S7-Xplorer but I have no idea whatsoever how to add any signal. Addressbook creator doesn't work at all, drag&drop as well. Could you give me some advice of how should I deal with this problem? Best regards! ------------------------------------------------------------------------------------------ |
Last edited by: Severus at: 11/20/2017 4:38:24 PMLast edited by: Jen_Moderator at: 11/21/2017 11:43:52 AMNew subject after splitting |
|
11/21/2017 12:53 AM | |
Posts: 2661 Rating: (279)
|
Have you checked the manuals? |
11/23/2017 5:50 AM | |
Joined: 10/7/2005 Last visit: 4/18/2024 Posts: 3003 Rating: (1046) |
Hello Severus a few pointers from my side: 1.) Based on your screendump you already have the latest ibaPDA version (V6.38.8 at time of posting) which is good as it now also also supports address book generation for S7-410 CPU's 2.) Multi Computing (more than 1 CPU in an S7-400 rack) should also work just fine with ibaPDA including S7 address book generation (certainly does for me) 3.) Please make sure to grab the latest ibaPDA-Interface-S7-Xplorer manual (V1.5 at time of posting) 4.) As for CFC: Silly question, did you do a complete compile of the charts and ticked "Generate SCL source"? (if not, please do so as it is needed for the ibaPDA address book, see chapter 3.4.5.3 of the ibaPDA-Interface-S7-Xplorer manual for more) 5.) Make sure to do a quick update of the the address book in ibaPDA whenever you make changes to your S7 project (its a simple single mouse click from the ibaPDA S7 symbol browser but required as the S7 address book in ibaPDA is not a "live link" to the S7 project) Hope this helps but by any means do also not hesitate to send a support enquiry to the iba Office in charge for your region in case of further problems. |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on