11/22/2017 3:32 PM | |
Joined: 7/30/2014 Last visit: 9/15/2024 Posts: 148 Rating: (1) |
Hi all, I am working in project with two servers (one master and other slave) and 8 clients. I made a copy (ghost) of the slave server and i put it in a new one, I removed the old slave server and replaced it with the new one changing the MAC and IP adress. First i got only the alarms and no data (as no link with the PLCs "S7-400") so to solve this i have followed this link https://support.industry.siemens.com/cs/ch/en/view/109743154 I got the data also the synchronisation between master and slave server see pic 1. Now my problem is that the master server doen't see the slave despite that synchronization occurs and when i want to switch to the slave server i can't see Pic2. The redundancy is done with terminal COM i tried it with ethernet but i got the same problem. see pic3 So what have i to do now? Best regards AttachmentPic1-2-3.docx (47 Downloads) |
Last edited by: sam2014 at: 11/22/2017 3:35:05 PMLast edited by: sam2014 at: 11/22/2017 3:36:39 PMLast edited by: Jen_Moderator at: 11/23/2017 9:38:42 AMInserted right link. |
|
11/26/2017 3:59 PM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2684) |
Hello sam; The following discussion might provide some hints: https://support.industry.siemens.com/tf/fr/en/posts/installation-of-cp1623/63017/?page=0&pageSize=10 Come back with information on the Simatic Net software version you have in your system. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
11/27/2017 8:47 AM | |
Joined: 7/30/2014 Last visit: 9/15/2024 Posts: 148 Rating: (1) |
thank you dchartier for reply, I have found a software and i have installed it finally my server works. Best regards, |
Follow us on