4/4/2017 6:19 PM | |
Joined: 9/28/2010 Last visit: 6/30/2024 Posts: 43 Rating: (8) |
I have this setup: S7-1511-1 PN (FW 2.0.5) <-> TP1200 Comfort (version 14.0.0.0) Step 7 Prof. V14, WinCC Advanced V14, TIA V14 Update 2 on Win 7 SP1 Professional. I have some system alarms in my plc. You can see them in attached picture PLCalarmsWeb.png. I can see them in the PLC webserver or I can see them on the small display on the 1511 CPU. Examples of the alarms: Error: Hardware component removed or missing PLC_1 (+R1.2-A1.1) / PS 25W 24VDC_1 (+R1.2-A1.0) I'm not sure what is the proper name of those alarms. System alarms? Diagnostics alarms? I would like to see those alarms in my Comfort panel in some normal Alarm view. I was following this manual, but it doesn't work. I'm not sure what alarm class should they be - the System, or the Diagnosis event. Anyway the desired alarms are not visible anywhere in my WinCC project or in the alarm view in runtime. I have the "S7 diagnostic alarms" checked in the Runtime Setting I have both classes (System and Diagnosis event) checked in my Alarm view. My System events list is imported, but it starts wit ID 9999 (and those desired alarms have ID like 31 or 33) My Controller alarms list is empty. Should they be here? Thanks for any help. Jan Jasek |
Follow us on