11/23/2017 8:59 AM | |
Posts: 17 Rating: (3) |
Hi, Currently I use STARTER V4.4.1.0. I have to tell that, when I was trying to connect the G120, I did not provide 380/400V for power unit, only 24V for logic unit. Without even opening the STARTER, when i turn on G120 e try to connect with it simply plugging the usb to one of whichever 4 usb port present on my field PG, PG can not recognize it. To explain, try immagine what is happening when you plug in a usb memory flash drive... It usually gets installed correctly. Here is the same thing except the fact that PG does not install a G120 driver. I've tried even to uninstall SIMATIC NET USB drivers and install them manually but with no success at all. From the first foto you can se that PG register editor does not "see" any USB Driver and yet in foto 2 you can se that there is one... Janko Attachmentfoto_usb.zip (56 Downloads) |
11/23/2017 9:19 AM | |
Posts: 17 Rating: (3) |
Hi, I think i do... See in attached photo. It should be G120C_PN; Janko |
11/23/2017 9:20 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
correct an now try to install the drivers then it should be displayed like this: |
11/23/2017 10:00 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, which driver and which driver version was installed? Regards Christoph |
Follow us on