10/12/2017 2:44 PM | |
Joined: 8/1/2007 Last visit: 8/29/2024 Posts: 1698 Rating: (84) |
Hello, I have the same configuration also on a Windows 7 Ultimate Industrial PC with 32 Bit. There I have only a CPU load of 36 - 44% What can it be that I have in the VM on the Windows 7 with 64Bit 100% CPU load? Best regarts Eleu Edit: I have found the Problem. I have stop the process and the CPU load is o.k. I have found this link about that: https://www.file.net/prozess/iastordatamgrsvc.exe.html I have deinstall the Intel(R) Rapid Storage Technology and it`s all all rigth. Best regarts Edit 2: On the industrial PC with Win 7 ultimate 32 Bit, I had to play back my data backup. Without this card driver, the Soft PLC always went into disorder and all the LEDs blinked. The test environment with Win 7 (64Bit) runs on a desktop PC. There the deainstallation was correct. |
Last edited by: Eleu at: 10/12/2017 3:02:39 PMLast edited by: Eleu at: 10/13/2017 1:51:33 PM |
|
2/20/2018 9:54 AM | |
Joined: 5/12/2006 Last visit: 9/23/2024 Posts: 22366 Rating: (3012) |
i see no picture! |
2/20/2018 1:11 PM | |
Joined: 4/10/2017 Last visit: 3/14/2023 Posts: 12 Rating: (0) |
i guess there are some server errors. I will try later.
|
Follow us on