8/31/2017 8:25 AM | |
Posts: 215 Rating: (6) |
I tried to dig into this matter some time ago. Look here for some further information. |
8/31/2017 7:43 PM | |
Posts: 3 Rating: (0) |
Hi JDarius, thank you for your help, but I'm still doing something wrong here. Could you try to identify? I tried to configure opcua server endpoint as 127.0.0.1 and as 192.168.10.100, wich is the IP of iot2040. In both cases UAExpert client says the same thing. I can't figure out what is wrong.
AttachmentDesktop.zip (903 Downloads) |
9/1/2017 7:51 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, have you already tried to use an example from the developers? You can find some here: https://github.com/mikakaraila/node-red-contrib-opcua/tree/master/examples You can try to run such an example with a server. If this is running you can use the code as basis for your application. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
2/17/2018 11:36 AM | |
Posts: 18 Rating: (0) |
Solved... it is working after installation of ntp Sync. Maybe it was a timestamp error best regards |
This contribution was helpful to1 thankful Users |
9/10/2018 1:30 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, you only can read out single items. You can use the OPC UA browser node to browse into the PLC. You can find an example here. I didn't manage it yet to browse down to the variables, maybe the code in the example has to be adapted.. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
7/12/2019 5:57 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by ak2923 is split to a separate thread with the subject IoT2020 as opc-server - How can access the variable? . Best regards |
7/12/2019 5:59 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by ak2923 is split to a separate thread with the subject Getting error when installing the opc ua package on the iot2020. Best regards |
Follow us on