2/17/2018 2:12 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello wimpy; Do you mean to say you have setup an IP address on the IM 153-1? how else would you try and ping it? What kind of Ethernet cable have you managed to connect to the IM 153-1? Sorry if i am being facetious, but what you are trying to do is not possible with that part number. The IM 153-1 is (exclusively) a Profibus-DP slave, an interface module for a remote I/O station on Profibus. It has no integrated interface for Ethernet, and does not accept an IP address. See the following screenshot showing part of the technical data for the IM 153-1, and open the following manual for more information:
https://support.industry.siemens.com/cs/dk/en/view/1142798 Hope this helps, Daniel Chartier |
2/17/2018 5:47 PM | |
Joined: 10/28/2014 Last visit: 4/17/2024 Posts: 63 Rating: (2) |
Hi Wimpy, Please note, Wincc V7.3 is not released for use with Windows10. Refer below link for supported OS. https://support.industry.siemens.com/cs/ww/en/view/97493192 Hope this helps! |
Last edited by: Jen_Moderator at: 2/19/2018 8:57:23 AMOptimized link. |
|
This contribution was helpful to1 thankful Users |
2/18/2018 4:59 AM | |
Posts: 19 Rating: (0) |
yes ET200 exclusive profibus, but CPU 315 PN DP. connect to 153. is not possible?? |
2/18/2018 8:56 AM | |
Joined: 10/28/2014 Last visit: 4/17/2024 Posts: 63 Rating: (2) |
Hi Wimpy, Refer the attached extract from manual for communication settings with PLC. Hope this Helps! AttachmentExtract_WinCC_Communication_en-US_en-US.pdf (142 Downloads) |
This contribution was helpful to1 thankful Users |
9/6/2018 6:21 AM | |
Posts: 19 Rating: (0) |
Thank's bro |
This contribution was helpful to1 thankful Users |
Follow us on