2/17/2018 10:06 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, and in your laptop with what? Excel? and which port have your laptop? one example: How do you create an OPC client with Microsoft Excel? - ID: 24299099 ... |
Last edited by: Ste39 at: 2/17/2018 10:14:51 PM |
|
2/17/2018 11:38 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Saurabh, ???? https://support.industry.siemens.com/tf/ww/en/posts/opc-ua-server/167780?page=0&pageSize=10 ??? |
Last edited by: Ste39 at: 2/17/2018 11:39:39 PM |
|
2/20/2018 4:38 PM | |
Joined: 8/3/2009 Last visit: 9/23/2024 Posts: 13759 Rating: (1738) |
Hello ssamber If you use a Simatic Net OPC Server from Siemens its an easy thing and in this case this is your FAQ: https://support.industry.siemens.com/cs/ww/en/view/67295801 But if you want to use a third party OPC Server then you have to contact the support tof this company they might have a manual or application example. Its because always the OPC Server to handle the connection to the field devices. Then you can use any OPC Client for getting the Data from the OPC Server. And as I wrote at the beginning the Simatic Net OPC Server can manage Connections to all S7 PLCs. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on