2/22/2018 12:22 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Hello gentlemen, I've been having some difficulty with what I thought DB_ANY but it turned out that my problems stem from using VarinatGet and TypeOf instructions in a program using s7-1214c Version 4.2. I'm programming with TIA14 -SP1 update 3 To make a long story shorter, I don't have access to an S7-1214C hardware at the moment and I'm simulating with PLCSIM. Does anyone know if there are issues using these instructions with S7-1200? I know they work well with s7-1500 but the manual states that they also work with s7-1200. Furthermore, the TypeOf instruction works in LAD but not in SCL and VariantGet doesn't work at all. I would like to know weather it's a simulator issue or a software bug. I have an archive of a small project with one block (FB4) if anyone has the time, access to S7-1200 and would be so kind as to test it on the hardware and let me know. The project also contains an S7-1500 program which works well in the simulator. Thanks Kal AttachmentVariantBug.zip (66 Downloads) |
2/22/2018 7:31 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Thanks #dp, it never dawned on me. Attached is an archive containing only s7-1200 project. Cheers Kal AttachmentVariantBug_Basic.zip (86 Downloads) |
2/22/2018 4:36 PM | |
Joined: 2/10/2012 Last visit: 9/18/2024 Posts: 314 Rating: (59) |
|
This contribution was helpful to2 thankful Users |
2/23/2018 3:23 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
EQ_Type screenshot |
This contribution was helpful to1 thankful Users |
Follow us on