11/17/2010 11:09 AM | |
Posts: 41 Rating: (0) |
Hello again, Is it possible to read R-parameters from channel 1 with NC-VAR selector, and if yes, which parameter should I choose? BR, Mitja |
11/17/2010 11:32 AM | |
Posts: 2964 Rating: (482) |
Hello.... Yes you can read the R-parameter from NC_Var selector. Details are attached in steps..... Check it out.... Regards, Ekalavya Ekalavya AttachmentRead_R_parameters.pdf (1332 Downloads) |
This contribution was helpful to3 thankful Users |
11/17/2010 12:52 PM | |
Posts: 41 Rating: (0) |
Gee Ekalavya, Thanks for your help, I hope it will work... BR, Mitja |
11/17/2010 1:05 PM | |
Posts: 41 Rating: (0) |
One more thing, I was a little bit confused, the real value I wanted to get is R220, hope this dosen't effect procedure? BR, Mitja |
3/15/2018 5:31 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello, Which machine data you want to read? Please refer SINUMERIK 840D sl/840Di sl/840D/840Di/810D System Variables manual & Read data from Sinumerik 840D NCU-Box (6FC5247-0AA00-0AA1) to 3rd party software for more detail information.
|
Last edited by: Jen_Moderator at: 3/15/2018 2:32:46 PMOptimized link. |
|
Follow us on