6/25/2018 4:00 PM | |
Joined: 12/12/2008 Last visit: 4/18/2024 Posts: 69 Rating: (6) |
Hi, There is two ways to connect to the IoT20x0 out of the box (with siemens example image) 1: SSH (i.e Putty, SSH to 192.168.200.1). 2: Serial cable, via X14 on PCB, under the right compartment "door", next to SD-card. Remember baud = 115200. If you dont have 115200 baud under "Serial" settings in putty, you WILL see garbage. /Ben |
This contribution was helpful to2 thankful Users |
6/26/2018 10:02 AM | |
Posts: 2 Rating: (0) |
my Baud Rate was incorrect, Thank You, very much appreciated :) |
Follow us on