6/22/2018 3:57 PM | |
Posts: 35 Rating: (1) |
Hello all, Plz tell me how to couple two motors (master slave) with parameter.plzz send in details. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/25/2018 10:26:44 AMNew subject after splitting |
|
6/24/2018 9:25 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
Hello, if you want to have an answer detail, please give also more details in your question (for example over your application). For axis couplings I see the following possibilities: 1.) simple torque coupling (used for very rigid mechanical couplings - for example two motors on one common mechanical shaft): You send the torque setpoint from the first axis directly to the slaves. Big advantages of the S120 with CU320 is, that you have no time delay between the axis. 2.) speed controlled- following an applications example: 3.) angular synchronism - standard mechanism with SIMOTION or S7-1500. Or you can do it inside the drive with DCB extension too: Zako |
6/25/2018 2:14 PM | |
Posts: 35 Rating: (1) |
dear sir, i have to couple two servo motors for rotary table on 828d system |
This contribution was helpful to1 thankful Users |
Follow us on