5/2/2017 5:25 PM | |
Posts: 158 Rating: (1) |
Can you confirm(see attached) that this is how to wire the AM2 AQ? It is very hard to find decent documentation for the wiring, and I don't want to burn this module up before I can use it. Also, on the "X11" row, there are 2 analog outputs with 2 terminals each? Is the rightmost terminal for earth ground? The diagrams are very vague. AttachmentAM2 AQ VFD SPEED.pdf (476 Downloads) |
5/2/2017 5:28 PM | |
Posts: 158 Rating: (1) |
|
7/19/2018 10:58 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Look at attachment |
7/19/2018 11:01 PM | |
Joined: 12/27/2006 Last visit: 4/25/2024 Posts: 1196 Rating: (113) |
Look in the attachment. So you connect a F.O. (VFD) to the LOGO module AM2 AQ The AM2 AQ module has 2 independent outputs, so you can use also U2+ and M2 And, you can (its not neccecary) use the X11 to connect it with the shield of the wiring Attachmentspeed2.pdf (330 Downloads) |
This contribution was helpful to2 thankful Users |
7/20/2018 6:19 AM | |
Joined: 10/20/2015 Last visit: 9/5/2023 Posts: 94 Rating: (19) |
Hello, Here is another one. |
This contribution was helpful to1 thankful Users |
Follow us on