10/21/2018 3:11 PM | |
Joined: 9/27/2006 Last visit: 9/24/2024 Posts: 12282 Rating: (2685) |
Hello Akbar; Based on this message, you should try to cantact Beijer to see if they have Lauer panel files in their archives: https://ssl.arcor-secure.de/systeme-lauer.de/sides/uebersicht/uebersicht_e.htm A .200 file is an old L2 network electronic file, L2 being an ancestor to Profibus-DP for S5 communications.. To read it you would need a COM ET200 software, integrated in Step 5. It seems that Lauer adapted this file so it could serve as a gsd file for their equipment But as you noticed it is extremely difficult to retrieve a .200 file on the web. If there is any way to contact the programmer of the original S7 program, he may still have a copy of this file; if you can open the original program, you will find it in the Step 7 files .../data/gsd/... directory. Hope this helps, Daniel Chartier |
10/22/2018 11:12 PM | |
Joined: 9/27/2006 Last visit: 9/24/2024 Posts: 12282 Rating: (2685) |
Hello Akbar; Before S7 PLCs there were S5 CPUs, and before Profibus Siemens had developped a similar network named L2-DP for S5 processors with interface modules IM 308A. The electronic data file for slaves on L2-DP was integrated with a separate software COM ET200, and had an extension .200. Eventually the network evolved to Profibus, the integration of the file was done with software COM Profibus and it was called a gsd file. But for a small period .200 files could be used for Profibus slave integration, with a S5 interface module IM 308B. That seems the case for your Lauer unit. One important question: are you sure about the designation of your Lauer PC807 HMI? There are links on the web for Lauer PCS-807 panels, with Profibus connection accessories, and software links. Possibly that is what you are really looking for? If this is the case, searching the web for PCS-807 would generte this type of answers. For example:
https://www.radwell.ca/Buy/LAUER%20SYSTEME/PCS807?redirect=true
https://www.vanegmond.nl/fileserver/Lauer/GSD-files,%20bouwstenen%20etc/SIEMENS/S7_200/PROFIBUS.DP/
Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
10/23/2018 5:46 AM | |
Joined: 6/14/2015 Last visit: 9/3/2024 Posts: 242 Rating: (2) |
Thank so much. Yes I saw all these web sites I need this GSD file , LAUSPC3X.200 But when I open this GSD file from this site I see this codes. Is it GSD file? or I need convert to GSD file? https://www.vanegmond.nl/fileserver/Lauer/GSD-files,%20bouwstenen%20etc/SIEMENS/S7_200/PROFIBUS.DP/ Is this GSD file? |
Last edited by: akbar_torkashwand at: 10/23/2018 5:49:15 AM |
|
10/28/2018 7:29 PM | |
Joined: 6/14/2015 Last visit: 9/3/2024 Posts: 242 Rating: (2) |
Thanks dchartierI sent Email to this web sitehttps://www.iae-service.de/(this site only open with Internet Explorer) They support Production of LAUERThey sent me GSD file that I need.I uploaded GSD file, maybe someone like me need it.Attachmentarchive.zip (955 Downloads) |
Last edited by: akbar_torkashwand at: 10/28/2018 7:30:25 PMLast edited by: akbar_torkashwand at: 10/28/2018 7:32:23 PMLast edited by: akbar_torkashwand at: 10/28/2018 7:33:23 PM |
|
This contribution was helpful to4 thankful Users |
Follow us on